T208x SRDS_PRTCL_S1 how to set?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T208x SRDS_PRTCL_S1 how to set?

1,010 次查看
gyosunshim
Contributor III

Hi All,

Use the T2080RDB evm board has designed the T2081 board.

SRDS_PRTCL_S1 value of T2080RDB is called to change this value to 0x66 0x6C.

How do I change the value?

Note also the boot to SD.

Thank you.

Best regards,

gyosun

标签 (1)
0 项奖励
回复
2 回复数

809 次查看
lunminliang
NXP Employee
NXP Employee

Hello gyosun shim,

Seems the question is not very clear.

The SRDS_PRTCL_S1is RCW field for setting Serdes protocol, please refer to Table 19-1 for SerDes Lanes Assignments.

You mentioned 0x66 0x6C, do you want to set one of this value?

You could use the QCVS tool to change this part in RCW and generate image.

Please correct me if this is not what you're asking about.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

809 次查看
gyosunshim
Contributor III

Hello lunminliang,

Please note that this question did not smooth.

I want to set the value to SRDS_PRTCL_S1 0x6c.

If QCVS tools have made the bin file, how do I download on u-boot?

I am using an SD card to boot.

Thank you,

Best regards,

gyosun

0 项奖励
回复