Dear freescale :
I want to reconfig and compile T2080 uboot to boot vxworks,
the sale give me QorIQ Linux SDK v2.0 PPC64E6500 Yocto Cache.iso,
I install it step by step,
but I can not get T2080 uboot source code , and do not know how to compile T2080 uboot
please tell me how to get T2080 uboot source code and compile it
thinks a lot !
hello ,
my question is , I need to work with uboot version v2014.01 , and later .
can you confirm it is what I need ,
how can verify I'm using the proper version?
thx
yuda
Hello Jiachao Zhang,
Please download Linux SDK 2.0 Source and Cache ISOs from Linux® SDK for QorIQ ® Processors|NXP , please install both ISOs "QorIQ Linux SDK v2.0 SOURCE.iso" and "QorIQ Linux SDK v2.0 PPCE6500 Yocto Cache.iso" in the same path.
Go to the folder <installation_path>/QorIQ-SDK-V2.0-20160527-yocto, create the build project and fetch u-boot source, modify and rebuild u-boot.
$ source ./fsl-setup-env -m t2080rdb
Get u-boot source code:
$ bitbake u-boot -c cleansstate
$ bitbake u-boot -c patch
Go to the u-boot source folder build_t2080rdb/tmp/work/t2080rdb-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git/ to modify u-boot source code according to your requirement.
Go back to folder build_t2080rdb to rebuild u-boot
$ bitbake u-boot
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hello ,
my question is , I need to work with uboot version v2014.01 , and later .
can you confirm it is what I need ,
how can verify I'm using the proper version?
thx
yuda