T2080 PVR Description

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 PVR Description

785件の閲覧回数
scottgerhold
Contributor IV

In the T2080 Reference Manual, section 7.3.4.1 PVR mentions that the register is described in DCFG_CCSR_PVR (section 27.3.11). But the field descriptions don't match. In 7.3.4.1 it calls bits 24:27 the Processor Major Revision # and 27.3.1 calls bits 16-23 the major revision #. Which table is correct?

ラベル(1)
0 件の賞賛
返信
1 返信

712件の閲覧回数
ufedor
NXP Employee
NXP Employee

Both variants are applicable considering that Chapter 7 is named "e6500 Core Integration", so the "Processor" here means "Core":

MAJOR_REV = Process revision + Manufacturing revision

MINOR_REV = Processor (Core) major revision number + Processor (Core) minor revision number

0 件の賞賛
返信