T2080 POWER SEQUENCING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 POWER SEQUENCING

836件の閲覧回数
aneeshk
Contributor I

Hi,

Is there any requirement of power sequencing in T2080 ,datasheet provides only the list of power rails?

ラベル(1)
タグ(1)
1 返信

743件の閲覧回数
r8070z
NXP Employee
NXP Employee

I could not say that the T2080 datasheet provides the list of power rails only.  Its section 3.2 “Power sequencing” clearly says that power rails must be applied in a specific sequence and requires all supplies be at their stable values within 400 ms.  Notice T2080 based  system may require the VDD supplies ramp prior to any of the I/O power. Because there is a brief period as the VDD powers up that the I/Os associated with applied  I/O supply may go from being  tristated to an indeterminate state (either driven to a logic one or zero).