T1022 IFC LSB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1022 IFC LSB

926件の閲覧回数
jack_mcculloch
Contributor I

Hi,

We would like to connect a TL16C752D Dual UART to the IFC bus on the T1022. We are assuming the GPCM mode is the most suitable for this application?

We are also unsure what LSB of address and data bus should be?

Should the address start at IFC_A31?

Is the Data bus LSB IFC_AD7 and MSB IFC_AD0?

ラベル(1)
0 件の賞賛
3 返答(返信)

901件の閲覧回数
jack_mcculloch
Contributor I

Thanks.

And how do we align the data bus if we are using 8 bits?

0 件の賞賛

895件の閲覧回数
r8070z
NXP Employee
NXP Employee

Connect 8-bit port  to AD[0:7], AD0 is the most significant bit.

 

0 件の賞賛

910件の閲覧回数
r8070z
NXP Employee
NXP Employee

In the normal GPCM mode of operation ADDR bus carries the least significant bits. ADDR[31] will carry the lsb of the system address.

0 件の賞賛