Rgmii to Rdmii connection in T1023

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rgmii to Rdmii connection in T1023

599 次查看
gauravverma
Contributor II

Can we make communication between two T1023 processor using direct  Rgmii interface?

Is this configuration is supported by software as well ?

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

481 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes, it is pssoble to connect two T1023 processors via RGMII directly (MAC-to-MAC connection). Software should be configured for fixed link when auto negation is disabled.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复