Rgmii to Rdmii connection in T1023

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rgmii to Rdmii connection in T1023

669 Views
gauravverma
Contributor II

Can we make communication between two T1023 processor using direct  Rgmii interface?

Is this configuration is supported by software as well ?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

551 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes, it is pssoble to connect two T1023 processors via RGMII directly (MAC-to-MAC connection). Software should be configured for fixed link when auto negation is disabled.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply