Dear NXP,
I am working on T4240RDB-64B machine. I needs to integrate NVRAM RTC (CY14B116M ) in build. I am using QORIQ-SDK-2.0 source.
Which one is suitable for this module or do I need to configure custom driver for this module ?
git/drivers/rtc/Makefile,
obj-$(CONFIG_DM_RTC) += rtc-uclass.o
obj-$(CONFIG_RTC_AT91SAM9_RTT) += at91sam9_rtt.o
obj-$(CONFIG_RTC_BFIN) += bfin_rtc.o
obj-y += date.o
obj-$(CONFIG_RTC_DAVINCI) += davinci.o
obj-$(CONFIG_RTC_DS1302) += ds1302.o
obj-$(CONFIG_RTC_DS1306) += ds1306.o
obj-$(CONFIG_RTC_DS1307) += ds1307.o
obj-$(CONFIG_RTC_DS1338) += ds1307.o
obj-$(CONFIG_RTC_DS1339) += ds1307.o
obj-$(CONFIG_RTC_DS1337) += ds1337.o
obj-$(CONFIG_RTC_DS1374) += ds1374.o
obj-$(CONFIG_RTC_DS1388) += ds1337.o
obj-$(CONFIG_RTC_DS1556) += ds1556.o
obj-$(CONFIG_RTC_DS164x) += ds164x.o
obj-$(CONFIG_RTC_DS174x) += ds174x.o
obj-$(CONFIG_RTC_DS3231) += ds3231.o
obj-$(CONFIG_RTC_FTRTC010) += ftrtc010.o
obj-$(CONFIG_SANDBOX) += i2c_rtc_emul.o
obj-$(CONFIG_RTC_IMXDI) += imxdi.o
obj-$(CONFIG_RTC_ISL1208) += isl1208.o
obj-$(CONFIG_RTC_M41T11) += m41t11.o
obj-$(CONFIG_RTC_M41T60) += m41t60.o
obj-$(CONFIG_RTC_M41T62) += m41t62.o
obj-$(CONFIG_RTC_M41T94) += m41t94.o
obj-$(CONFIG_RTC_M48T35A) += m48t35ax.o
obj-$(CONFIG_RTC_MAX6900) += max6900.o
obj-$(CONFIG_RTC_MC13XXX) += mc13xxx-rtc.o
obj-$(CONFIG_RTC_MC146818) += mc146818.o
obj-$(CONFIG_RTC_MCP79411) += ds1307.o
obj-$(CONFIG_MCFRTC) += mcfrtc.o
obj-$(CONFIG_RTC_MK48T59) += mk48t59.o
obj-$(CONFIG_RTC_MPC5200) += mpc5xxx.o
Thanks & Regards,
VinothS
已解决! 转到解答。
Please refer to [05/11] rtc: add generic nvmem support - Patchwork to customize NVRAM RTC driver.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Please refer to [05/11] rtc: add generic nvmem support - Patchwork to customize NVRAM RTC driver.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------