Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

跳至解决方案
1,382 次查看
Larry5335
Contributor IV

Has the T2080RDB been verified to operate with a 16GB DIMM or larger?

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,140 次查看
Bulat
NXP Employee
NXP Employee

I am not sure if it has been varified, however it should be ok with 16GB DIMM.

I think "larger" size is not applicable to the T2080RDB, main restriction is the number of ranks. iI maximum it supports dual-rank SODIMM, or in other words only two CS's are connected to the SODIMM socket and 16GB is the maximum size.

Regards,

Bulat

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,141 次查看
Bulat
NXP Employee
NXP Employee

I am not sure if it has been varified, however it should be ok with 16GB DIMM.

I think "larger" size is not applicable to the T2080RDB, main restriction is the number of ranks. iI maximum it supports dual-rank SODIMM, or in other words only two CS's are connected to the SODIMM socket and 16GB is the maximum size.

Regards,

Bulat

0 项奖励
回复