Connecting nor flash with t2080 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Connecting nor flash with t2080 processor

跳至解决方案
1,563 次查看
agxinj
Contributor I

Hai

         I am using t2080 QorIQ Series processor in my design ,I found in the reference schematic that the flash chip connected to t2080 (data line0 is connected to data pin 15 of flash chip )

why is this reversal  in connectivity.Is there any specific reason ?

regards

AGXIN.J

标签 (1)
0 项奖励
1 解答
1,320 次查看
Bulat
NXP Employee
NXP Employee

Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.

Regards

在原帖中查看解决方案

0 项奖励
1 回复
1,321 次查看
Bulat
NXP Employee
NXP Employee

Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.

Regards

0 项奖励