Connecting nor flash with t2080 processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connecting nor flash with t2080 processor

ソリューションへジャンプ
1,562件の閲覧回数
agxinj
Contributor I

Hai

         I am using t2080 QorIQ Series processor in my design ,I found in the reference schematic that the flash chip connected to t2080 (data line0 is connected to data pin 15 of flash chip )

why is this reversal  in connectivity.Is there any specific reason ?

regards

AGXIN.J

ラベル(1)
0 件の賞賛
1 解決策
1,319件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.

Regards

元の投稿で解決策を見る

0 件の賞賛
1 返信
1,320件の閲覧回数
Bulat
NXP Employee
NXP Employee

Yes, PowerPC and Power ISA architectures have a specific feature, Most Significant Bit (MSB) has index 0. So IFC_AD[0] is the MSB on the bus and it should be connected to MSB of the NOR flash, that is DQ[15]. This expalins "reversal" in connectivity on the IFC bus.

Regards

0 件の賞賛