Hi All,
I am working on T4240RDB. As per document (QORIQ-SDK-2.0-IC-REV0.pdf) I flash the Linux image 0xE8020000. I needs to flash the Linux image to 0XE8000000.
I needs to configure the Linux address, Will you please tell me the which files to configure the Linux Address ?
Regards,
VinothS
Thank you Ufedor,
We have two NOR Flash chip So, Address start from 0XE0000000 and RCW hard-coded in this address as per my customer.
I want to know the files to configure the Linux address. I will check and conform from my side.
Thanks & Regards,
VinothS,
You wrote:
> We have two NOR Flash chip
What is the projected NOR Flash subsystem memory map?
Are chip-selects connected to the Flash devices fixed or they can be swapped?
> I want to know the files to configure the Linux address.
The Linux uImage address is not configured in files.
We are talking about U-Boot uImage binary object which can be programmed anywhere in the boot ROM
The uImage has built-in header containing RAM loading parameters - Data Load Address and Entry Point Address.
The "0xE8020000" is not used inside uImage.
Thank you Ufedor,
If I changed Linux Address in bootcmd.
> This is just Linux.uImage address. It is not configured. It is used in the bootcmd only
Board is not boot, stop in u-boot and provide the "Cannot get kernel Image"
initcall: eff4ecacHit any key to stop autoboot: 0
WARNING: adjusting available memory to 30000000
Wrong Image Format for bootm command
ERROR: can't get kernel image!
Regards,
VinothS.