Hello everyone, I have just started working on a new T4240 QDS board. I have the board failing in the U-boot sequence immediately after detecting the DDR3 ram ("Waiting for D_INIT timeout. Memory may not work."). and the configuration switches and U-Boot booting log as below,and the three 8G DDR3-1866 UDIMM are installed in J23-D2_DIMM#1,
J22-D1_DIMM#1,J200-D3_DIMM#1,however I try to change the SW1 to 0x24,and update the bank4 Uboot to SDK-V1.8 and SDK-V1.9 version,but the issue same before,Any suggestions for this boot issue?thanks!
SW1= 0x17; SW2= 0xfe; SW3= 0x0c; SW4= 0x50; SW5= 0xe2; SW6= 0x0f; SW7= 0xea; SW8= 0xcd; SW9= 0x1f;
U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 15 2013 - 18:54:15)
CPU0: T4240E, Version: 2.0, (0x82480020)
Core: E6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:733.333 MHz,
DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz
FMAN1: 733.333 MHz
FMAN2: 733.333 MHz
QMAN: 366.667 MHz
PME: 533.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 16070019 18101916 00000000 00000000
00000010: 04383060 30548c00 ec020000 f5000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000028
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x14, vBank: 0
FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
Detected UDIMM
Detected UDIMM
Waiting for D_INIT timeout. Memory may not work.
22 GiB left unmapped
DDR: 24 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 3-way 4KB
DDR Chip-Select Interleaving Mode: CS0+CS1
Solved! Go to Solution.
Hello Lei zhihua,
There should be no problem with software, please refer to my following u-boot log.
Please download T4240QDS Quick start from http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...to check whether you plugged in DDR DIMMs correctly. In addition, please make sure that you used all the DDR3 DIMMs provided together with t4240QDS board.
If your problem remains, please contact your local FAE to check the hardware for you.
U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 16 2013 - 11:20:16)
CPU0: T4240E, Version: 2.0, (0x82480020)
Core: E6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:733.333 MHz,
DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz
FMAN1: 733.333 MHz
FMAN2: 733.333 MHz
QMAN: 366.667 MHz
PME: 533.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 16070019 18101916 00000000 00000000
00000010: 04383060 30548c00 ec020000 f5000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000028
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x12, vBank: 4
FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
Detected UDIMM
Detected UDIMM
22 GiB left unmapped
DDR: 24 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 3-way 4KB
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage 1030 mV
Flash: 128 MiB
L2: 2048 KB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1536 KB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 28 (0x1c)
Using SERDES3 Protocol: 6 (0x6)
Using SERDES4 Protocol: 12 (0xc)
SRIO1: enabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
EEPROM: NXID v1
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe260000
02:00.0 - 8086:10d3 - Network controller
PCIe3: Bus 01 - 02
PCIe4: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Data at eff40000 is not a firmware
e1000: 68:05:ca:0f:23:a3
e1000#0
Warning: e1000#0 MAC addresses don't match:
Address in SROM is 68:05:ca:0f:23:a3
Address in environment is 00:e0:0c:00:ae:00
Hit any key to stop autoboot: 0
=>
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi @leizhihualqytvw , @yipingwang
Have you been resolve this problem. I had the trouble the same as you with custom board use b4860.
Thanks and brgs
Hello leizhihua LQYTVWF,
According to your u-boot log, this error indicates there is hardware or frequency configuration on your target. Please check switch setting and RCW configuration.
Please configure SW7 : 0xFA = 11111010, and use RCW from Linux SDK pre-built ISO, please refer to the attachment.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,Yiping Wang,
I try it with SW7:0xFA & attach rcw file,and the issue same as before,When I remove the 8G UDIMM in J200-D3_DIMM#1 the Uboot to normal work as below,however When I install the UDIMM to J200-D3_DIMM#1 or J201-D3_DIMM#2 the Uboot will show "Waiting for D_INIT timeout. Memory may not work."
Is not a D3_DIMM memory controller hardware problems?thanks for your feedback.
U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 15 2013 - 18:54:15)
CPU0: T4240E, Version: 2.0, (0x82480020)
Core: E6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:733.333 MHz,
DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz
FMAN1: 733.333 MHz
FMAN2: 733.333 MHz
QMAN: 366.667 MHz
PME: 533.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 16070019 18101916 00000000 00000000
00000010: 04383060 30548c00 ec020000 f5000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000028
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x14, vBank: 0
FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
Detected UDIMM
There is no rank on CS0 for controller 2.
Not all controllers have compatible interleaving mode. All disabled.
14 GiB left unmapped
DDR: 16 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage 1033 mV
Flash: 128 MiB
L2: 2048 KB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1536 KB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 28 (0x1c)
Using SERDES3 Protocol: 6 (0x6)
Using SERDES4 Protocol: 12 (0xc)
SRIO1: enabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (08bafd4d != 00000000)
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, no link, regs @ 0xfe260000
PCIe3: Bus 01 - 01
PCIe4: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.4.10
Failed to connect
Failed to connect
Fman2: Uploading microcode version 106.4.10
FM1@DTSEC5 [PRIME], FM2@DTSEC5
Hit any key to stop autoboot: 10 0
Hello Lei zhihua,
There should be no problem with software, please refer to my following u-boot log.
Please download T4240QDS Quick start from http://www.nxp.com/products/microcontrollers-and-processors/power-architecture-processors/qoriq-powe...to check whether you plugged in DDR DIMMs correctly. In addition, please make sure that you used all the DDR3 DIMMs provided together with t4240QDS board.
If your problem remains, please contact your local FAE to check the hardware for you.
U-Boot 2013.01QorIQ-SDK-V1.5 (Dec 16 2013 - 11:20:16)
CPU0: T4240E, Version: 2.0, (0x82480020)
Core: E6500, Version: 2.0, (0x80400120)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:733.333 MHz,
DDR:933.333 MHz (1866.667 MT/s data rate) (Asynchronous), IFC:183.333 MHz
FMAN1: 733.333 MHz
FMAN2: 733.333 MHz
QMAN: 366.667 MHz
PME: 533.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 16070019 18101916 00000000 00000000
00000010: 04383060 30548c00 ec020000 f5000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000028
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x12, vBank: 4
FPGA: v6 (T4240QDS_2014_0211_1852), build 547 on Wed Feb 12 00:52:40 2014
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM
Detected UDIMM
Detected UDIMM
22 GiB left unmapped
DDR: 24 GiB (DDR3, 64-bit, CL=13, ECC on)
DDR Controller Interleaving Mode: 3-way 4KB
DDR Chip-Select Interleaving Mode: CS0+CS1
VID: Core voltage 1030 mV
Flash: 128 MiB
L2: 2048 KB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1536 KB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 28 (0x1c)
Using SERDES3 Protocol: 6 (0x6)
Using SERDES4 Protocol: 12 (0xc)
SRIO1: enabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
*** Warning - bad CRC, using default environment
EEPROM: NXID v1
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe260000
02:00.0 - 8086:10d3 - Network controller
PCIe3: Bus 01 - 02
PCIe4: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Data at eff40000 is not a firmware
e1000: 68:05:ca:0f:23:a3
e1000#0
Warning: e1000#0 MAC addresses don't match:
Address in SROM is 68:05:ca:0f:23:a3
Address in environment is 00:e0:0c:00:ae:00
Hit any key to stop autoboot: 0
=>
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,Yiping Wang,
I double check all configuration with Quick start document,and the issue same as before,Maybe it's hardware issue as you said,i will contact with your local team,however thanks for your kind support!
Lei zhihua