Can not use kexec with SDK 2.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can not use kexec with SDK 2.0

2,106件の閲覧回数
ivankoveshnikov
Contributor I

We have an issue with loading the Linux kernel using kexec tool.The Idea was to first boot T4240RDB board using default device tree and then reboot into usdpaa enabled version. Tested on T4240RDB, Linux 4.1.8-rt8, SDK-2.0 . 

 

But kexec can not load device tree blob (dtb) file. We have done several experiments on kexec with certain amount of the load options, none of them was successful. For more detailed information look below:


Linux kernel was reconfigured to set desired options:
CONFIG_HOTPLUG_CPU=y
CONFIG_KEXEC=y
CONFIG_CRASH_DUMP=y
CONFIG_CMDLINE="root=/dev/sda1 rw console=ttyS0,115200 ramdisk_size=1000000 fsl_fm_max_frm=9600 bportals=s0-1 qportals=s0-1 rootwait reset_devices"

 

1. Reboot from non-usdpaa to non-usdpaa configuration
Try to load kernel with "--dtb" and "--command-line" options set.
# kexec -l /boot/vmlinux-4.1.8-rt8 --dtb=/boot/devicetree-uImage-t4240rdb.dtb --command-line="`cat /proc/cmdline`"

# kexec -e
In this example the Linux tries to reboot but it seems, that cmdline was set as an empty string: no output to console, no any other effect (see kexec1.txt)

 

2. Reboot from non-usdpaa to non-usdpaa configuration
Try to load kernel with only "--command-line" option set. 
# kexec -l /boot/vmlinux-4.1.8-rt8 --dtb=/boot/devicetree-uImage-t4240rdb.dtb --command-line="`cat /proc/cmdline`"

# kexec -e

In this case kexec report about modifying cmdline, and then i can see kernel booting. But output is full of straces, and after boot I have no network interfaces available (see kexec2.txt)

Original Attachment has been moved to: kexec2.txt.zip

Original Attachment has been moved to: kexec1.txt.zip

ラベル(1)
0 件の賞賛
返信
1 返信

937件の閲覧回数
zhengruoqin
Contributor I

Well, I have the same problem with SDK2.0-1703 on ls1046.

0 件の賞賛
返信