Bring up custom T1024 Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bring up custom T1024 Board

489 次查看
abhishekborana
Contributor II

Hi.. I am facing difficulty to bring up T1024 custom board. The board has 2GB DDR3L RAM using 9 discrete chips. CPLD is absent on custom board. I was able to program flash. But the program do not run. Asleep pin is high and I am not using heat sink

0 项奖励
1 回复

389 次查看
Bulat
NXP Employee
NXP Employee

A lot of issues can cause problems to board functionality. First of all check that all power supplies are ok, the system clock is as expected, POR configuration settings are ok and RCW are read correctly.

Absence of a heat sink can cause device overheating.

Regards,

Bulat

0 项奖励