Booting from SPI NAND Flash on T1014

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting from SPI NAND Flash on T1014

1,107件の閲覧回数
tukimukai_th10
Contributor I

Hello,

Is it possible to use SPI NAND Flash as a boot device on T1014 processor?

Thanks in advance,
Hirobe

ラベル(1)
0 件の賞賛
5 返答(返信)

1,000件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes, it is possible.

0 件の賞賛

1,000件の閲覧回数
tukimukai_th10
Contributor I

As an additional question, can you also support the additional configuration needed for using u-boot to boot SPI NAND Flash?
Or is it possible to booting from SPI NAND Flash based on existing the T1024RDB configuration and code of SPI Flash boot?

Thanks in advance,

Hirobe

0 件の賞賛

1,000件の閲覧回数
ufedor
NXP Employee
NXP Employee

The following three points need to be considered for serial NAND device to support booting from it:
• Support 0x03 READ command.
• Support 24-bit address mode when the device boots from the QuadSPI interface.

0 件の賞賛

1,000件の閲覧回数
tukimukai_th10
Contributor I

Thank you for your supporting.

I'll check u-boot configure(RCW, defconfig, etc...) and source code for booting from SPI based on your advice.

hirobe

0 件の賞賛

1,000件の閲覧回数
tukimukai_th10
Contributor I

Thank you for your quick support.

Hirobe

0 件の賞賛