Best evaluation board for QorIQ T1022 processor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Best evaluation board for QorIQ T1022 processor?

Jump to solution
911 Views
kaitav_sapre
Contributor I

Hi,

We are looking at QorIQ T1022 as our potential processor and would like to know the best evaluation board for it. We will be using DDR4 RAM, Gigabit Ethernet, PCIe interfaces, etc., so the evaluation board should support them.

I came across the following boards on the NXP website which seem suitable:

#1. QorIQ® T1040 Reference Design Board: QorIQ® T1040 Reference Design Board | NXP 

#2. QorIQ T1042 DEVELOPMENT SYSTEM, DDR4 MEMORY: T1042D4RDB-PA Product Information|NXP 

Based on my quick scan, it seems that #2 would be our best bet. However, when I click on the "Product Summary" link, I get nagivated to #1, QorIQ® T1040 Reference Design Board. 

Where do I get details of the T1042D4RDB-PA evaluation board? 

Could anyone please suggest the best option?

Any help is much appreciated. Thank you!

Labels (1)
1 Solution
807 Views
ufedor
NXP Employee
NXP Employee

T1042D4RDB is the best option - for the documentation please refer to:

QorIQ® T1040 Reference Design Board | NXP 

View solution in original post

2 Replies
808 Views
ufedor
NXP Employee
NXP Employee

T1042D4RDB is the best option - for the documentation please refer to:

QorIQ® T1040 Reference Design Board | NXP 

807 Views
kaitav_sapre
Contributor I

Okay, thanks a lot. 

0 Kudos
Reply