Hi;
i'm currently trying to register CW, and would like to use a usb dongle as license ID.
I followed the instruction from the FAQ (Licensing and Registration FAQ), explaining how to install FLEXlm and USB Dongle Driver, which i downloaded from the following page: USB Dongle Drivers.
Thus, i'm using a computer that is running Windows 7, 32bits. It seems that the USB dongle driver available on the FSL web page is for Windows XP only.
The chapter "Updates and Patches" is empty, so there is no other version of the driver. I've tried to use it, but the LMtools lives the FLEXID field empty. It's exactly like there is no USB dongle...
Does anyone knows how to get the correct version of the USB dongle driver?
Thanks in advance,
Mitch
已解决! 转到解答。
Hi Tomas,
it will likely be 2+ months to have a new FlexLM installer that can be used with dongles and Win7. if you have an immediate need, I have attached temporary licensing until the new installer gets created. the License is through Nov 30th
Regards,
Hi Thomas.
Our current dongle drivers do not function with Windows 7 and the older CW IDE we are working to get this fix as soon as possible. but in the meantime can you tell me if you are you using the Eclipse Version of CodeWarrior?
Regards,
Hi Jorge,
thanks for your answer.
Note: i answer you directly, because i can't login to the forum anymore...
We are using Codewarior, version 5.1, as builder, and as IDE as well. We don't have Eclipse.
What are the delay for the Windows7 version of the dongle driver, because we would like to buy another usb dongle?
Regards,
Michel
========================================
Message du 28/09/12 00:25
De : "jorge_plascencia"
A : "Michel Thomas"
Copie à :
Objet : Re: CodeWarrior Licensing - USB dongle driver for Windows 7
Freescale Community
USB dongle driver for Windows 7 created by jorge_plascencia in CodeWarrior Licensing - View the full discussion
Hi Thomas. Our current dongle drivers do not function with Windows 7 and the older CW IDE we are working to get this fix as soon as possible. but in the meantime can you tell me if you are you using the Eclipse Version of CodeWarrior?
Regards, Reply to this message by replying to this email -or- go to the message on Freescale CommunityStart a new discussion in CodeWarrior Licensing by email or at Freescale Community
Hi Jorge,
many thanks for your support and for the license file.
I'm looking forward for the updates of the license tools.
Regards,
Michel
========================================
Message du 01/10/12 21:04
De : "jorge_plascencia"
A : "Michel Thomas"
Copie à :
Objet : Re: CodeWarrior Licensing - USB dongle driver for Windows 7
Freescale Community
USB dongle driver for Windows 7 created by jorge_plascencia in CodeWarrior Licensing - View the full discussion
Hi Tomas, it will likely be 2+ months to have a new FlexLM installer that can be used with dongles and Win7. if you have an immediate need, I have attached temporary licensing until the new installer gets created. the License is through Nov 30th
Regards,
Reply to this message by replying to this email -or- go to the message on Freescale CommunityStart a new discussion in CodeWarrior Licensing by email or at Freescale Community