Hello CodeWarrior Support,
I am using a very similar setup with Coder Warrior V10.6.4 as my colleagues:
Windows 7 64Bit
USB license Dongle
Of course I installed the FLEXId_D.exe drivers and the FSLFlexLMinstall.exe.
Checking the licence manager (lmtool.exe) I can see the correct FLEXID which matches the licene.dat file.
I can even see the status "activated" in the CW IDE Help-> Page -> Freescale Licenses Page.
But after I run my compilation command over the console (toolchain does not use IDE) I still get the error:
"ERROR L4025: This limited version allows only 65536 bytes of C code"
I already double checked the installation reinstalled compiler, drivers and flexlm sw the same way my collegues did but still face the same license error.
Somehow I suspect an unfortunate constellations of different license dongles/files in my system which I also need besides CW.
Can someone give me a hint on how to solve this issue. Because based on the retrieved FLEXID and correct license status in the IDE it seems not to be a driver issue.
Thank you for your support!
Best regards
Alex
解決済! 解決策の投稿を見る。
Finally I was able to solve my problem. Indeed it was an issue with another compiler which uses FLEXlm license management via floating server. After experimenting with FLEXlm services with console commands I was able to see that the environmental variable LM_LICENSE_FILE was not set to the license.dat and therfore FLEXIds have not matched.
If you use any other FLEXLM related compiler/tool double check your LM_LICENSE_FILE environment variable and add the correct path of the licence.dat.
Hi,
I follow specification(below link) to generate licence.bat with usb Dongle. But code warrior shows error info when I debug codes. Could you please help to tell how to generate license which can be used to debug successfully? Thanks.
http://www.nxp.com/assets/documents/data/en/supporting-information/DongleQS.pdf
Finally I was able to solve my problem. Indeed it was an issue with another compiler which uses FLEXlm license management via floating server. After experimenting with FLEXlm services with console commands I was able to see that the environmental variable LM_LICENSE_FILE was not set to the license.dat and therfore FLEXIds have not matched.
If you use any other FLEXLM related compiler/tool double check your LM_LICENSE_FILE environment variable and add the correct path of the licence.dat.