Licensing for CW10.1 Special Edition for Kinetis

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Licensing for CW10.1 Special Edition for Kinetis

ソリューションへジャンプ
3,476件の閲覧回数
Niall
Contributor II

When I try to build a project in CW10_MCU_V10.1_SE I get a message saying my application could not obtain a license file. I though that the special edition did not require a license file.

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,740件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,741件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

0 件の賞賛
返信
1,740件の閲覧回数
joker441
Contributor I

same here...

0 件の賞賛
返信
1,740件の閲覧回数
Niall
Contributor II

I would like to add some more information on my previous post. I have installed the Special Edition of CW10.1 for windows (CW10_MCU_V10.1_SE). When I try to build one of the Kinetis example projects I get a Flexnet License Finder error saying that a license can't be obtained. The screenshot is attached. My understanding is that the Special edition of Codewarrior does not need a registered license and that a license file is installed during installation. My installation directory does not contain a license.dat file.

 

Has anybody else come across the same problem? I am trying to figure out if it is an installation problem or a bug in the special edition.

0 件の賞賛
返信
1,740件の閲覧回数
moat
Contributor I

error still exists...

 

Downloading eval now.

0 件の賞賛
返信
1,740件の閲覧回数
kef
Specialist I

Did you see last post to this thread ?:

https://community.freescale.com/thread/80580

0 件の賞賛
返信
1,740件の閲覧回数
olebon
Contributor I

I am having the same problem. I guess it will never be solved :smileysad: The only solution is to remove this retarded CW and use IAR instead.

 

 

PS Just added "FLEXLM_BATCH= -add 1" to the eclipse config file, this helped. Decided to keep CW :smileyhappy:

0 件の賞賛
返信
1,740件の閲覧回数
emh203
Contributor II

I have experienced this too.   I amusing the evaluation edition for now....

0 件の賞賛
返信