FLEXlm USB Dongle Program Installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXlm USB Dongle Program Installation

2,364 Views
Keith4DSmith
Contributor V

I am having difficulty with the USB Dongle installation procedure.

 

1 - The documentation that comes with the USB dongle is significantly out of date.

     a - The documentation states to download HASP_User_Setup_5[1].11.zip.

     When one follows the path through the websites [www.freescale.com/Code Warrior Development Tools/Licensing and Registration/Flexm Downloads/USB Dongle Drivers

        one ends up downloading the file FlexId_D.exe, not the zip file mentioned above.

     b - The issue with FlexId_D.exe is that the program is only for Windows XP and before. The installation does run on Windows 7, but nothing is installed.

 

     c - I would bring to your attention that a similar question was written in Oct. 2012. Nothing was posted that the problem was resolved. USB dongle driver for Windows 7

 

Is there a better program available for USB dongles used with CodeWarrior?

Labels (1)
0 Kudos
Reply
2 Replies

1,327 Views
Rick_Li
NXP Employee
NXP Employee

Hi Keith,

you are right, in general, for Windows 7 system, there is no need to install the driver for USB Dongle.

the below is the link for USB Dongle drivers.

the lmtools can be used for manage the USB dongle.

USB Dongle Drivers|Freescale

0 Kudos
Reply

1,326 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

HI Keith,

sorry for the old data you got from the document I have attached a most recent document that can help you with your question.

Regards,

0 Kudos
Reply