Code Warrior 5.1 do't show CAN components in PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code Warrior 5.1 do't show CAN components in PE

575件の閲覧回数
Anonymous
適用対象外

Dear Sir,

 

I have project in MC9s12G48 which have CAN component but it does't open in my CW5.1

I unable to see CAN component in processor expert .

 

Please help me.

Thanks in advance

 

rishi

ラベル(1)
0 件の賞賛
返信
1 返信

462件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I think you don't have the right license file.

There are 2 beans supporting the CAN:

    Init_MSCAN  under Peripheral Initialization Components which is included in all suites.

    FreescaleCAN is an Advanced Components which is included in Professional suite only.

You can order the bean separately too.

    Embedded Components|Freescale

By default under Processor Expert you've a "licensed" tab.

Only the beans validated by the license file are listed.

If you click on this tab you will have access to all beans.

However if you add the FreescaleCAN bean without having the right license file, no code will be generated for this bean.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信