How to install/use USBdongle license under Win 8.1?
Configuration used:
Native installation Win 7 Enterprise 64 bit
Oracle VM VirtualBox V4.3.28 r 100309
Windows 8.1 Enterprise 64 bit
This doc will answer the question:
Can we use USBdongle license under Win 8.1 ?
There are 2 parts:
Attached you will find 2 videos explaining the processes.
Refer to the USBDongle_driver_installation.avi
BEFORE Phase 4, to avoid problem we recommend to un-plug ethernet cable or switch-off wifi.
If network connection is not switched-off, for Phase 4 and Phase 5, a wrong driver could be installed.
Right Driver version (USBDongle + FlexID Driver installed + Windows 7 64bit)
To test it I used:
- CW for MPC55XX V2.7
Refer to the USBDongle_win8_MPC55XX.avi
- CW for HC12 V5.1
Refer to the USBDongle_win8_hc12v5.1.avi
Include example project -> HC12_V5_1_test_project.zip
Hope this will help.
Pascal