wakeup and sleep mode of fxls8962

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wakeup and sleep mode of fxls8962

1,424件の閲覧回数
lyp06118022
Contributor I

Hi,

I am using fxls8962 through freedom sensor Toolbox . I want to activate the sleep mode. what I do just as the following:

0X17, SENS-CONFIG3 = 0X80, 12,5HZ WAKEUP,  3200HZ  SLEEP (default in FRDM)

0x18, SENS-CONFIG4 =0X21, WAKE SDCD_OT, ACTIVATE _HIGH;

0X1E, ASLP_CNT_LSB = 96;

0X20, INT_EN =0X84, DATA READY and ASLP EN;

0x30, SDCD_CONFIG2 = 0XD8, default value, SDCD_EN

SDCD value is -125~125.

when I kick start, the sensor can read the XYZ data periodically in the "accelerometer" page, and I can see the INT1 interrupt from the oscilloscope. And it  can go to sleep mode itself after 8s just as the setting. And the sys_mode is truly =0x2, means is in sleep mode now. However, when I shake the freedom sensor, I can read the sys_mode turns to =0x01, means is wakeup now. But in the "accelerometer" page there is no data update, no INT1 interrupt from oscilloscope.

the BT-mode = GND ( the same as my MCU board)

what I want is: the sensor can wakeup itself from sleep mode, and Activate INT1/INT2 interrupt, so my main MCU can be activated through interrupt from sleep mode.

So, is there any other steps I need to do to finish the sleep mode setting? Thank you.

Best regards,

li yanpo

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,333件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Li Yanpo,

please find AN12004 attached, where you can find examples for setting FXLS89x2 accelerometers in different modes.

With Best Regards,

Jozef 

0 件の賞賛
返信