Hi Parth,
Attached you can find the source code for the FRDM-KL26Z board and the MPL115A2 pressure sensor on the KITMPL115A2I2C board. It is written in the CW for MCU's v10.6 and uses the I2C1 module (PTC1 and PTC2 pins) for I2C communication. Both the pressure and temperature are calculated in the infinite while loop:
while(1)
{
I2C_WriteRegister(MPL115A2_I2C_ADDRESS, CONVERT_REG, 0x00); // Start pressure and temperature conversion
Pause(0x17B2); // Wait ~4ms (3ms is a minimum delay)
I2C_ReadMultiRegisters(MPL115A2_I2C_ADDRESS, Padc_MSB_REG, 4, RawPressureTempData); // Read raw pressure and temperature data
// Temperature calculation
Tadc = ((uint16_t) (RawPressureTempData[2]<<8 | RawPressureTempData[3])) >> 6;
Temperature = (605.75 - Tadc) * 0.186916;
// Pressure calculation
Padc = ((uint16_t) (RawPressureTempData[0]<<8 | RawPressureTempData[1])) >> 6;
c12x2 = (((float) C12) / 4194304) * Tadc;
a1 = (((float) B1) / 8192) + c12x2;
a1x1 = a1 * Padc;
y1 = (((float) A0) / 8) + a1x1;
a2x2 = (((float) B2) / 16384) * Tadc;
Pcomp = y1 + a2x2;
Pressure = (Pcomp * 65 / 1023) + 50;
Pause(0xFFFF);
}
and can be watched in the "Variables" window on the top right of the Debug perspective:
I hope it helps.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.
Hi Parth,
Attached you can find the source code for the FRDM-KL26Z board and the MPL115A2 pressure sensor on the KITMPL115A2I2C board. It is written in the CW for MCU's v10.6 and uses the I2C1 module (PTC1 and PTC2 pins) for I2C communication. Both the pressure and temperature are calculated in the infinite while loop:
while(1)
{
I2C_WriteRegister(MPL115A2_I2C_ADDRESS, CONVERT_REG, 0x00); // Start pressure and temperature conversion
Pause(0x17B2); // Wait ~4ms (3ms is a minimum delay)
I2C_ReadMultiRegisters(MPL115A2_I2C_ADDRESS, Padc_MSB_REG, 4, RawPressureTempData); // Read raw pressure and temperature data
// Temperature calculation
Tadc = ((uint16_t) (RawPressureTempData[2]<<8 | RawPressureTempData[3])) >> 6;
Temperature = (605.75 - Tadc) * 0.186916;
// Pressure calculation
Padc = ((uint16_t) (RawPressureTempData[0]<<8 | RawPressureTempData[1])) >> 6;
c12x2 = (((float) C12) / 4194304) * Tadc;
a1 = (((float) B1) / 8192) + c12x2;
a1x1 = a1 * Padc;
y1 = (((float) A0) / 8) + a1x1;
a2x2 = (((float) B2) / 16384) * Tadc;
Pcomp = y1 + a2x2;
Pressure = (Pcomp * 65 / 1023) + 50;
Pause(0xFFFF);
}
and can be watched in the "Variables" window on the top right of the Debug perspective:
I hope it helps.
Regards,
Tomas
PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.