mm9z1_638 A B BOOT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mm9z1_638 A B BOOT

580 次查看
a852013777
Contributor III

Hi NXP partner

 

We would like to update firmware by canbus for mm9z1_638. Can we separate the flash to A & B partition ,and MM9Z1_638 can switch A partition or B partion for boot? thanks

 

Br,

Mike liang

 

0 项奖励
回复
2 回复数

562 次查看
prakashram72
Contributor III

Hi @a852013777 

Yes, you can partition the flash into A and B partitions for the MM9Z1_638. The MM9Z1_638 has a feature called 'Flash Swap' which allows you to switch between two different firmware images stored in separate partitions of the flash memory. This can be useful for firmware updates via CAN bus.

To implement this, you would need to configure the Flash Swap Control Register (FSCR) to enable the Flash Swap feature and set the Swap Indicator Address (SIA) to the start address of the B partition. When a reset occurs, the MM9Z1_638 will check the SIA and if it is set, it will boot from the B partition. If the SIA is not set, it will boot from the A partition.

Here is a code snippet that shows how to configure the FSCR and SIA:

 // Enable Flash Swap FSCR |= FSCR_FSWPEN_MASK;
// Set Swap Indicator Address to start of B partition SIA = B_PARTITION_START_ADDRESS;

Please refer to the MM9Z1_638 reference manual for more details on the Flash Swap feature and how to configure the FSCR and SIA. You can find the reference manual in the MagniV Microcontrollers section of the community.nxp.com website.

 

Hope this helps!

0 项奖励
回复

552 次查看
a852013777
Contributor III

@prakashram72 

Hi prakashram 

I cannot  get the referece manual from the link. Could you send mail to me or update the link?

My email: mike.yh.liang.foxconn.com

Please refer to the MM9Z1_638 reference manual for more details on the Flash Swap feature and how to configure the FSCR and SIA. You can find the reference manual in the MagniV Microcontrollers section of the community.nxp.com website.

 

Br,

Mike Liang

0 项奖励
回复