Hi ,
Im using mag3110 .Im readin die_temp register succesfully .But when Im heating sensor up , the "continously reading data " is not updating .When I switch off sensor -shut down- and run it again then it is updating ?
How can I update it while it is running?
Thanks
已解决! 转到解答。
Hello Murat,
As per your description it looks like the sensor is in “STANDBY” mode. Please take a look at note #2 in page 13 of the datasheet:
http://cache.freescale.com/files/sensors/doc/data_sheet/MAG3110.pdf
"Register contents are preserved when transitioning from “ACTIVE” to “STANDBY” mode."
Please make sure that the sensor is in "ACTIVE" mode otherwise you'd be always reading the same value.
Once you have a valid value in the temperature register, remember that the die temperature sensor is not factory trimmed (as stated by the datasheet). This should be included in the errata soon. You can get around this by trimming the output by software.
Hope it helps =)
Hello Murat,
As per your description it looks like the sensor is in “STANDBY” mode. Please take a look at note #2 in page 13 of the datasheet:
http://cache.freescale.com/files/sensors/doc/data_sheet/MAG3110.pdf
"Register contents are preserved when transitioning from “ACTIVE” to “STANDBY” mode."
Please make sure that the sensor is in "ACTIVE" mode otherwise you'd be always reading the same value.
Once you have a valid value in the temperature register, remember that the die temperature sensor is not factory trimmed (as stated by the datasheet). This should be included in the errata soon. You can get around this by trimming the output by software.
Hope it helps =)