Will a 12V voltage supply kill a MPX5050?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will a 12V voltage supply kill a MPX5050?

489件の閲覧回数
garvin
Contributor I

Will a 12V voltage supply kill a MPX5050 pressure sensor? Or, will it only effect the reading of the pressure?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

329件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Jia Gao,

The required voltage supply for the sensor should be between 4.75V and 5.25V, powering the integrated sensor at different voltage (12V in this case) than the specified in the datasheet can probably not kill the pressure sensor (I cannot warranty that) but is not recommended because the offset, temperature coefficient of offset (TCO) and temperature coefficient of span (TCS) trim will be invalidated and will affect the sensor accuracy and veracity.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

329件の閲覧回数
garvin
Contributor I

Thank you, Jose.

0 件の賞賛
返信