TSUP on MM912J637

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,794件の閲覧回数
igw
Contributor II

Hello all,

The MM912J637 has a low current voltage output intended to drive an external temperature sensor, TSUP, as well as a dedicated ADC.

The specs for TSUP show a +/-5% variation around the nominal 1.25V.

I am wondering if I need to account for this voltage tolerance in my temperature accuracy calculations *or* if the TSUP voltage is related to the ADC's VREF.

So, in effect my question is, is the ADC doing a ratiometric or absolute measurement on the voltage at VTEMP.

How closely does TSUP track VREF is probably the most telling specification (and is not in the datasheet)?

Thanks,

Ian

ラベル(1)
0 件の賞賛
返信
1 解決策
1,376件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,377件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

0 件の賞賛
返信