TSUP on MM912J637

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TSUP on MM912J637

跳至解决方案
1,634 次查看
igw
Contributor II

Hello all,

The MM912J637 has a low current voltage output intended to drive an external temperature sensor, TSUP, as well as a dedicated ADC.

The specs for TSUP show a +/-5% variation around the nominal 1.25V.

I am wondering if I need to account for this voltage tolerance in my temperature accuracy calculations *or* if the TSUP voltage is related to the ADC's VREF.

So, in effect my question is, is the ADC doing a ratiometric or absolute measurement on the voltage at VTEMP.

How closely does TSUP track VREF is probably the most telling specification (and is not in the datasheet)?

Thanks,

Ian

标签 (1)
0 项奖励
回复
1 解答
1,216 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,217 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ian,

The reference of the External Temp Sensor is TSUP.

This means that for external temperature measurement the variation of TSUP will not impact the measurement.

Regards,

Tomas

0 项奖励
回复