Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

跳至解决方案
1,198 次查看
roberto70
Contributor I

What samplerate is FRDM-KL26Z_MQXL.hex that is included with the Freescale Vibration Monitor using for the FXOS8700? Since the software displays frequencies up to 400Hz I assume the maximum possible samplerate of 800Hz is used. Am I right? I'm asking since I see significant differences to my own FXOS8700 implementation on vibrations above 30Hz.

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,030 次查看
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,030 次查看
roberto70
Contributor I

Arrrggh, could have answered that myself. There is a sample each other 1.25ms so the samplerate is 800Hz. Sorry for asking.

0 项奖励
回复
1,031 次查看
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

0 项奖励
回复
1,030 次查看
roberto70
Contributor I

Thank you!

0 项奖励
回复