Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Samplerate of FXOS8700 using FRDM-KL26Z_MQXL.hex

ソリューションへジャンプ
1,958件の閲覧回数
roberto70
Contributor I

What samplerate is FRDM-KL26Z_MQXL.hex that is included with the Freescale Vibration Monitor using for the FXOS8700? Since the software displays frequencies up to 400Hz I assume the maximum possible samplerate of 800Hz is used. Am I right? I'm asking since I see significant differences to my own FXOS8700 implementation on vibrations above 30Hz.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,790件の閲覧回数
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,790件の閲覧回数
roberto70
Contributor I

Arrrggh, could have answered that myself. There is a sample each other 1.25ms so the samplerate is 800Hz. Sorry for asking.

0 件の賞賛
返信
1,791件の閲覧回数
JackITB
NXP Employee
NXP Employee

Correct,

Some more details are mentionned in the Help tab, paragraph 5:Sensors

0 件の賞賛
返信
1,790件の閲覧回数
roberto70
Contributor I

Thank you!

0 件の賞賛
返信