Questions for receiving the NTM88 example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions for receiving the NTM88 example

737件の閲覧回数
israelfelix
Contributor III

To configure my RF receiver, I need the settings present in the NTM88 example code such as: carrier frequency (434MHz? Could it be 433.92MHz?), transmission rate (maximum 19200 bauds?), but mainly the deviation. Another question is whether the CRC sent uses all values as 1 or as 0?

0 件の賞賛
返信
5 返答(返信)

715件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Israel,

for the code examples to the NTM88, please refer to the NTM88 product page. The code examples are under the Software part.

JozefKozon_0-1712819525165.png

 

With Best Regards,

Jozef

0 件の賞賛
返信

711件の閲覧回数
israelfelix
Contributor III

Thanks for the answer! I already have the code example, I'm looking for the NTM88's default RF settings, specifically whether the CRC sends 0 or 1, and the derivation value when at 433mhz.

0 件の賞賛
返信

632件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Israel,

please see below an answer from the application engineer.

DESCRIPTION

The default values of the registers are indicated in the user manual. See the “Reset” row in the register description: it contains the values of the different bits when the RF block is turned ON.

JozefKozon_0-1713170590084.png

 

With Best Regards,

Jozef

0 件の賞賛
返信

690件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Israel,

please see below an answer from an application engineer I have contacted.

DESCRIPTION

The RF block is initialized in the u8InitRf() function located in main.c

This is where the registers controlling the frequency, baud rate, frequency deviation… are configured.

JozefKozon_0-1712895947075.png

To see the correspondence between register values and frequency, baud rate… please refer to the user manual which details all registers:

https://www.nxp.com/webapp/Download?colCode=UM11227&appType=license

With Best Regards,

Jozef

685件の閲覧回数
israelfelix
Contributor III

Thank you Josef for trying to help me with the problem! Reading the code, check that there is the following account explained: "434.0083 - 433.9131 = +/- 47.6kHz" Would this be the derivation rate of the central frequency? Or is it related to BFREQ/AFREQ = 3.17 kHz?

0 件の賞賛
返信