Nomenclature available for KMI rotational sensor series?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Nomenclature available for KMI rotational sensor series?

648 次查看
michellecunniff
Contributor I

Is there a nomenclature available for KMI rotational sensor series? Or an explaination available eg: KMI16 / KMI25?

标记 (2)
0 项奖励
3 回复数

520 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, there is no document which explains the product naming, Sorry about that.

But I will try to help. You can find a very general information about how to identify the NXP rotational sensors from our current portfolio:

KMI16:

3-pin package, Rotational sensor.

Output voltage with open collector.

KMI17:

2-pin package, Rotational sensor.

Two-wire current interface technology.

KMI23:

2-pin package, High performance rotational speed sensor (dedicated to ABS applications).

Two wire current interface technology.

KMI25:

3-pin, High performance rotational speed sensor (dedicated to ABS applications).

Two wire current interface technology.

Digital input which converts an external resistance into a one-bit signal.

Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

520 次查看
michellecunniff
Contributor I

Hi Jose,

Thank you for that information! So can I take it that there is no logic

behind the numbering ie: 15, 16, 17?

Also, is there a document for the product naming of OH403 etc (Conti

versions) again rotational sensors?

Thanks for your help, I really appreciate it.

Have a good day,

Michelle

0 项奖励

520 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Michelle,

Correct, there is no logic behind the numbering.

 

OH403 is not a public device, so, answering to your question: no, there is no document for product naming of OH403.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励