Hi,
Unfortunately, there is no document which explains the product naming, Sorry about that.
But I will try to help. You can find a very general information about how to identify the NXP rotational sensors from our current portfolio:
KMI16:
3-pin package, Rotational sensor.
Output voltage with open collector.
KMI17:
2-pin package, Rotational sensor.
Two-wire current interface technology.
KMI23:
2-pin package, High performance rotational speed sensor (dedicated to ABS applications).
Two wire current interface technology.
KMI25:
3-pin, High performance rotational speed sensor (dedicated to ABS applications).
Two wire current interface technology.
Digital input which converts an external resistance into a one-bit signal.
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jose,
Thank you for that information! So can I take it that there is no logic
behind the numbering ie: 15, 16, 17?
Also, is there a document for the product naming of OH403 etc (Conti
versions) again rotational sensors?
Thanks for your help, I really appreciate it.
Have a good day,
Michelle
Hi Michelle,
Correct, there is no logic behind the numbering.
OH403 is not a public device, so, answering to your question: no, there is no document for product naming of OH403.
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------