NTM88 external sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTM88 external sensor

490件の閲覧回数
Jpernia89
Contributor I

Hi guys,

I'll like to add a temperature sensor beside the one that this uC comes with. How can I do that? is there an option for one wire connection for interfacing a sensor like DS18B20? or how can i send a spi data to the NTM88 for RF transmitting (I'm thinking of connecting Low power uC with a sensor and sending it to the NTM88 via spi). Or the possibility to connect analog sensor to the NTM88.

 

 

0 件の賞賛
返信
2 返答(返信)

413件の閲覧回数
Sebastian-Jaimes
Contributor I

Hello guys, I still got the question, if I want to add an external temperature sensor to the NTM88, but it has no IIC, is it posible to use the ADC that comes with the NTM88?

0 件の賞賛
返信

481件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

We don't have one wire connection temp sensor,but IIC interface instead.

I3C/I²C Digital Temperature Sensors | NXP Semiconductors

タグ(1)
0 件の賞賛
返信