Hi,
When RFCR3_FNUM is >0, the transmission of multiple frames is enabled. In this case, the same frame is transmitted multiple times. It is not possible to change the content of the frame between two transmissions.
In order to send several frames with a different content each time, the following sequence can be implemented:
To monitor the end of the transmission, bits RFCR7_RFIF and RFCR7_RFEF can be polled if an interrupt-based method is not possible.
After the transmission has been triggered, bit RFIF will be set at the end of the transmission, if successful. If not successful, bit RFEF will be set.
After a transmission has completed, do not forget to clear RFIF/RFEF bit by setting RFIAK bit.
BR, Tomas
Hi,
When RFCR3_FNUM is >0, the transmission of multiple frames is enabled. In this case, the same frame is transmitted multiple times. It is not possible to change the content of the frame between two transmissions.
In order to send several frames with a different content each time, the following sequence can be implemented:
To monitor the end of the transmission, bits RFCR7_RFIF and RFCR7_RFEF can be polled if an interrupt-based method is not possible.
After the transmission has been triggered, bit RFIF will be set at the end of the transmission, if successful. If not successful, bit RFEF will be set.
After a transmission has completed, do not forget to clear RFIF/RFEF bit by setting RFIAK bit.
BR, Tomas
Hi Tomas
I can't get it to work using interrupts and polling, it works using delays. But the delay time is not well calculated and it affects the program operation. Are there other registers that are not configured properly?