MPR03x pad shape/area

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPR03x pad shape/area

ソリューションへジャンプ
1,985件の閲覧回数
onechil
Contributor II

The app. note in the link below suggests suggests that "The minimum pad size for Freescale’s products is 3 mm by 3 mm when using thin film overlays to about 0.5 mm thickness of acrylic or ABS plastic".

In a proximity sensing application, assuming the area of the object to be sensed is >= 9mm sq. and the profile of the object is planar to the sensing electrode pad on a PCB, is it accurate to interpret the 3mm x 3mm recommendation, as a 9mm sq. minimum electrode pad area for Freescale's touch sensing products?

Thanks,

ラベル(1)
1 解決策
1,646件の閲覧回数
Joshevelle
Senior Contributor I

Hello onechil,

Yes.

Proximity sensors like the MPR03x sense changes in the Electrode Capacitance, which is related to the electrode's area. We suggest a minimum of 3x3mm which equals to 9mm sq area. So yes, you shouldn't have any issues.

Hope it helps.

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,647件の閲覧回数
Joshevelle
Senior Contributor I

Hello onechil,

Yes.

Proximity sensors like the MPR03x sense changes in the Electrode Capacitance, which is related to the electrode's area. We suggest a minimum of 3x3mm which equals to 9mm sq area. So yes, you shouldn't have any issues.

Hope it helps.

Josh

0 件の賞賛
返信
1,646件の閲覧回数
onechil
Contributor II

Hi Joshevelle,

Sounds good! I thought as much, but wanted some clarification, cheers.

1,646件の閲覧回数
Joshevelle
Senior Contributor I

You're welcome. Have fun!

Josh

0 件の賞賛
返信
1,646件の閲覧回数
onechil
Contributor II

Actually I have one more question - I haven't been able to find a recommended PCB footprint for the MPR03x uDFN part. Would you be able to refer me to one? Thanks.

0 件の賞賛
返信