MM9Z1_638 XTAL no signal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MM9Z1_638 XTAL no signal

跳至解决方案
918 次查看
a852013777
Contributor III

Hi Nxp Partner

We try to write firware code when we get our first version senior board (installs MM9Z1_638).

We found EXTAL& XTAL is oscillation signal and We also check all the voltage pin of MM9Z1_638 (VDDA,VDDX,VDDH,VDD2D,LTO ,RESET) is within the spec's requirement.Do you have any suggestion to check why EXTAL& XTAL no signal?

 

Br,

Mike Liang

0 项奖励
1 解答
911 次查看
a852013777
Contributor III

hi jozef

Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?

"without  extal signal"can we wirte firmware to mm9z1_638 now ?

 

Br 

Mike liang 

在原帖中查看解决方案

0 项奖励
3 回复数
915 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Mike,

please check the OSCE bit in the CPMUOSC register. It should be set to 1 to see an external wave on the EXTAL pin.

JozefKozon_0-1663838436469.png

JozefKozon_1-1663838463181.png

With Best Regards,

Jozef

0 项奖励
912 次查看
a852013777
Contributor III

hi jozef

Should we use ic programmer to write initial firmware to mm9z1_638 before mount on pcb?

"without  extal signal"can we wirte firmware to mm9z1_638 now ?

 

Br 

Mike liang 

0 项奖励
894 次查看
a852013777
Contributor III

hi jozef

We add 470nf on two reset pin. We can write firmware. thanks 

 

Br,

Mike Liang