MC33771

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771

4,140 Views
sujendra_n2
Contributor I

Hi,

We are using the logic of XOR the data with polynomial and saving the reminder as CRC.

But we are not getting the CRC and Tomas vaverka sent text file on that with usage of 0x42 as seed.

I don't know why this seed and please let me know the logic how are you calculating.

Thanks and Regards

N Sujendra

This message contains information that may be privileged or confidential and is the property of the KPIT Technologies Ltd. It is intended only for the person to whom it is addressed. If you are not the intended recipient, you are not authorized to read, print, retain copy, disseminate, distribute, or use this message or any part thereof. If you receive this message in error, please notify the sender immediately and delete all copies of this message. KPIT Technologies Ltd. does not accept any liability for virus infected mails.

0 Kudos
Reply
4 Replies

1,644 Views
jcsansao
Contributor II

Dear all, 

This is the code I´m using:

mc33771_crc8.c ---->


// ------------------------------------------------------------------
#include "mc33771_crc8.h"
// ------------------------------------------------------------------
static const uint8 crc_table[256] = {
0x00, 0x2f, 0x5e, 0x71, 0xbc, 0x93, 0xe2, 0xcd, 0x57, 0x78, 0x09, 0x26, 0xeb, 0xc4, 0xb5, 0x9a,
0xae, 0x81, 0xf0, 0xdf, 0x12, 0x3d, 0x4c, 0x63, 0xf9, 0xd6, 0xa7, 0x88, 0x45, 0x6a, 0x1b, 0x34,
0x73, 0x5c, 0x2d, 0x02, 0xcf, 0xe0, 0x91, 0xbe, 0x24, 0x0b, 0x7a, 0x55, 0x98, 0xb7, 0xc6, 0xe9,
0xdd, 0xf2, 0x83, 0xac, 0x61, 0x4e, 0x3f, 0x10, 0x8a, 0xa5, 0xd4, 0xfb, 0x36, 0x19, 0x68, 0x47,
0xe6, 0xc9, 0xb8, 0x97, 0x5a, 0x75, 0x04, 0x2b, 0xb1, 0x9e, 0xef, 0xc0, 0x0d, 0x22, 0x53, 0x7c,
0x48, 0x67, 0x16, 0x39, 0xf4, 0xdb, 0xaa, 0x85, 0x1f, 0x30, 0x41, 0x6e, 0xa3, 0x8c, 0xfd, 0xd2,
0x95, 0xba, 0xcb, 0xe4, 0x29, 0x06, 0x77, 0x58, 0xc2, 0xed, 0x9c, 0xb3, 0x7e, 0x51, 0x20, 0x0f,
0x3b, 0x14, 0x65, 0x4a, 0x87, 0xa8, 0xd9, 0xf6, 0x6c, 0x43, 0x32, 0x1d, 0xd0, 0xff, 0x8e, 0xa1,
0xe3, 0xcc, 0xbd, 0x92, 0x5f, 0x70, 0x01, 0x2e, 0xb4, 0x9b, 0xea, 0xc5, 0x08, 0x27, 0x56, 0x79,
0x4d, 0x62, 0x13, 0x3c, 0xf1, 0xde, 0xaf, 0x80, 0x1a, 0x35, 0x44, 0x6b, 0xa6, 0x89, 0xf8, 0xd7,
0x90, 0xbf, 0xce, 0xe1, 0x2c, 0x03, 0x72, 0x5d, 0xc7, 0xe8, 0x99, 0xb6, 0x7b, 0x54, 0x25, 0x0a,
0x3e, 0x11, 0x60, 0x4f, 0x82, 0xad, 0xdc, 0xf3, 0x69, 0x46, 0x37, 0x18, 0xd5, 0xfa, 0x8b, 0xa4,
0x05, 0x2a, 0x5b, 0x74, 0xb9, 0x96, 0xe7, 0xc8, 0x52, 0x7d, 0x0c, 0x23, 0xee, 0xc1, 0xb0, 0x9f,
0xab, 0x84, 0xf5, 0xda, 0x17, 0x38, 0x49, 0x66, 0xfc, 0xd3, 0xa2, 0x8d, 0x40, 0x6f, 0x1e, 0x31,
0x76, 0x59, 0x28, 0x07, 0xca, 0xe5, 0x94, 0xbb, 0x21, 0x0e, 0x7f, 0x50, 0x9d, 0xb2, 0xc3, 0xec,
0xd8, 0xf7, 0x86, 0xa9, 0x64, 0x4b, 0x3a, 0x15, 0x8f, 0xa0, 0xd1, 0xfe, 0x33, 0x1c, 0x6d, 0x42
};
// ------------------------------------------------------------------
/*! \brief Calculates the CRC8 and appends it as data[data_len] to buffer.
*
*/
void appendcrc8(uint8 *data, uint16 data_len) {
uint8 tbl_idx;
uint8 crc;

crc = 0x42; // seed

while (data_len--) {
tbl_idx = ((crc >> 0) ^ *data) & 0xff;
crc = (crc_table[tbl_idx] ^ (crc << 8)) & 0xff;

data++;
}
*data = crc & 0xff;
}
// ------------------------------------------------------------------
/*! \brief Calculates the CRC8 and returns it.
* return 0 if CRC is correct
* *
*/
uint8 checkcrc8(uint8 *data, uint16 data_len) {
uint8 tbl_idx;
uint8 crc;

crc = 0x42; // seed

while (data_len--) {
tbl_idx = ((crc >> 0) ^ *data) & 0xff;
crc = (crc_table[tbl_idx] ^ (crc << 8)) & 0xff;

data++;
}
return crc & 0xff;
}

mc33771_crc8.h---->

#ifndef MC33771_CRC8_H_
#define MC33771_CRC8_H_

#include "PE_Types.h"

void appendcrc8(uint8 *data, uint16 data_len);
uint8 checkcrc8(uint8 *data, uint16 data_len);

#endif /* MC33771_CRC8_H_ */

Best Regards!

0 Kudos
Reply

1,644 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sujendra,

The SEED is 11111111.

The “0x42” is coming from the CRC table. Maybe the comment is not well done.

Best regards,

Tomas

PS: There is no need to create another thread, next time please just update the original one.

0 Kudos
Reply

1,644 Views
sujendra_n2
Contributor I

Hi,

We have Evaluation board(KIT33771TPLEVB) of MC33771A and we need to connect one device through SPI.

Is it possible through SPI for single device or need to use TPL.

@please help in this we need to test our software today.

Thanks and Regards

N Sujendra

+919986513265

0 Kudos
Reply

1,644 Views
sujendra_n2
Contributor I

Hi,

In MC33771A how ow much time it will take to complete conversion of adc to read data in measurement registers?

0 Kudos
Reply