Do MPXV5100GC6U can be used as water-pressure sensor ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do MPXV5100GC6U can be used as water-pressure sensor ?

1,528 次查看
steventwu
Contributor I

From the datasheet, I can't confirm that this sensor can be used for water-pressure detection .

Do anyone can help me? or it only use for air-pressure detection.

标签 (1)
0 项奖励
回复
1 回复

908 次查看
miguelsalhuana
NXP Employee
NXP Employee

Steven,

The MPX5100 can be used to measure tank levels by using the column of air method. The sensor will read the change in pressure in the column of air as the tank fills or empties. The sensor is not manufactured to be submerged in water.

Regards,

Miguel

0 项奖励
回复