Do MPXV5100GC6U can be used as water-pressure sensor ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do MPXV5100GC6U can be used as water-pressure sensor ?

1,317 Views
steventwu
Contributor I

From the datasheet, I can't confirm that this sensor can be used for water-pressure detection .

Do anyone can help me? or it only use for air-pressure detection.

Labels (1)
0 Kudos
1 Reply

697 Views
miguelsalhuana
NXP Employee
NXP Employee

Steven,

The MPX5100 can be used to measure tank levels by using the column of air method. The sensor will read the change in pressure in the column of air as the tank fills or empties. The sensor is not manufactured to be submerged in water.

Regards,

Miguel

0 Kudos