Difference between MPL3115A2 and MPL3115A2S

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Difference between MPL3115A2 and MPL3115A2S

跳至解决方案
294 次查看
CL_ENVEA
Contributor I

Hello,

 

I am wondering what is the difference between MPL3115A2 and MPL3115A2S

I can't tell why there is a change in reference as the datasheet seems identical.

Thanks in advance,

0 项奖励
回复
1 解答
290 次查看
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

在原帖中查看解决方案

0 项奖励
回复
2 回复数
291 次查看
CL_ENVEA
Contributor I

I got a quick reply from the tech support: 100% compatible, just a new fab

0 项奖励
回复
281 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear CL_ENVEA,

yes, this is correct. It is the same component. Thank you for posting the answer here, for other customer's convinience.

With Best Regards,

Jozef

0 项奖励
回复