Difference between FXL and MMA sensors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Difference between FXL and MMA sensors

700 次查看
monstor
Contributor II

I am choosing a G-sensor for our project development.

1. I would like to know the difference between FXL and MMA G-sensor?

2. Can these sensor support Roll over function or I need to calculate the roll over angle by myself?

Thank you very much.

0 项奖励
回复
1 回复

550 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Henry Wu,

Answering to your first question regarding the difference between FXL and MMA in our accelerometers naming, there are no functionality changes, is more related to the part number schemes, basically all of our “older” part number accelerometers starts with MMA and the newest accelerometers part numbers starts with “FXL”.

For your second question regarding the Roll Over Function, according to my understanding a car roll over is basically searching for a quick change in the angulation of the vehicle and it involves forces from 2g to 8g, please correct me if I’m wrong.

Unfortunately none of the Freescale accelerometers have embedded the function of rollover detection, so you would need to calculate it by yourself, however, you can probably use the detection of change of tilt angle exceeding a threshold of the embedded Vector-Magnitude function on the FXLS8471Q as described in the application note AN4692: www.freescale.com/files/sensors/doc/app_note/AN4692.pdf

This Application note comes with an associated software that you can download from the following link: www.freescale.com/files/sensors/doc/app_note/AN4692SW.zip

I hope this helps.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复