Difference between FXL and MMA sensors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between FXL and MMA sensors

704 Views
monstor
Contributor II

I am choosing a G-sensor for our project development.

1. I would like to know the difference between FXL and MMA G-sensor?

2. Can these sensor support Roll over function or I need to calculate the roll over angle by myself?

Thank you very much.

0 Kudos
Reply
1 Reply

554 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Henry Wu,

Answering to your first question regarding the difference between FXL and MMA in our accelerometers naming, there are no functionality changes, is more related to the part number schemes, basically all of our “older” part number accelerometers starts with MMA and the newest accelerometers part numbers starts with “FXL”.

For your second question regarding the Roll Over Function, according to my understanding a car roll over is basically searching for a quick change in the angulation of the vehicle and it involves forces from 2g to 8g, please correct me if I’m wrong.

Unfortunately none of the Freescale accelerometers have embedded the function of rollover detection, so you would need to calculate it by yourself, however, you can probably use the detection of change of tilt angle exceeding a threshold of the embedded Vector-Magnitude function on the FXLS8471Q as described in the application note AN4692: www.freescale.com/files/sensors/doc/app_note/AN4692.pdf

This Application note comes with an associated software that you can download from the following link: www.freescale.com/files/sensors/doc/app_note/AN4692SW.zip

I hope this helps.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply