Can NXP provide dual-frequency ——315/434 MHZ hardware circuit design?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can NXP provide dual-frequency ——315/434 MHZ hardware circuit design?

618 次查看
yangmingsong
Contributor II

Customer wants to develop 315/434 dual frequency tire pressure sensor with FXTH87EH116T1.

Can NXP provide dual-frequency hardware circuit design?

标签 (1)
0 项奖励
回复
1 回复

569 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mingsong,

Please find below the answer from our TPMS RF expert:

I never realized a common 315MHz-434MHz matching network as I generally optimize both frequency (for CZ context in particular), therefore two matching networks are usually worked out. Nevertheless it is something that can be envisage, but with few dBs losses on each frequency.

 

I attach a document showing the location of impedances that have to be presented to the RF pin for both frequency. Depending whether you have access to the RF pin directly (probe station) or by means of a SMA connector as I proceed myself, impedances are reported within this document.

Best regards,

Tomas

0 项奖励
回复