Are FXTH87 and FXTH87E codes(.s19 file) compatible

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Are FXTH87 and FXTH87E codes(.s19 file) compatible

跳至解决方案
1,061 次查看
jack_wang
Contributor I

Hello.

    Are FXTH87 and FXTH87E codes(.s19 file) compatible?

    If I can't use FXTH87 code(.s19 file) directly on FXTH87E, where do I need to change it?

 

                                                Jack Wang

0 项奖励
1 解答
936 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jack,

The firmware of FXTH87 can directly be used in FXTH87E. There is only one modification to perform in case there are pressure or acceleration threshold values in the application code. In the FXTH87E, the pressure and acceleration transfer functions have been modified compared to the FXTH87. This means that the same number of pressure or acceleration counts, for both raw and compensated measurement, do not represent the same pressure and acceleration value. This implies that in the application code, threshold values for pressure and acceleration must be re-calculated. The conversion formula from counts to g or kPa is given in the datasheet.

The attached slides illustrate the change of transfer function.

 

Updating the pressure and acceleration threshold values is the only modification to perform to adapt to the FXTH87E. Everything else remains the same as the FXTH87.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
2 回复数
937 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jack,

The firmware of FXTH87 can directly be used in FXTH87E. There is only one modification to perform in case there are pressure or acceleration threshold values in the application code. In the FXTH87E, the pressure and acceleration transfer functions have been modified compared to the FXTH87. This means that the same number of pressure or acceleration counts, for both raw and compensated measurement, do not represent the same pressure and acceleration value. This implies that in the application code, threshold values for pressure and acceleration must be re-calculated. The conversion formula from counts to g or kPa is given in the datasheet.

The attached slides illustrate the change of transfer function.

 

Updating the pressure and acceleration threshold values is the only modification to perform to adapt to the FXTH87E. Everything else remains the same as the FXTH87.

Best regards,

Tomas

0 项奖励
936 次查看
jack_wang
Contributor I

Hello Tomas

    Thank you very much!

                      Jack Wang

0 项奖励