Hi,
I want to integrate se05x-4.3.1 recipe into mickledore yocto source code(6.1.55 Linux Kernel) for imx8mm-lpddr4-evk target board.
I haved downloaded "se05x_mw_v04.05.00.zip" from below link and try to compiling se05x_4.3.1.bb file
I tried to compile se05x-4.3.1.bb recipe, during do_package stage, recipe failed "libcrypto.a" : not a valid ELF file. Please find attached logs for more details
Error Logs as follow :-
Initialising tasks: 100% |###############################################################################################################| Time: 0:00:09
Sstate summary: Wanted 615 Local 609 Mirrors 0 Missed 6 Current 4399 (99% match, 99% complete)
NOTE: Executing Tasks
ERROR: se05x-4.3.1-r0 do_package: dwarfsrcfiles failed with exit code 1 (cmd was ['dwarfsrcfiles', '/home/stackadmin/mallikarjuna/master/build/tmp/work/armv8a-poky-linux/se05x/4.3.1-r0/package/home/root/se05x_mw_v04.03.01/simw-top/ext/openssl/lib_mingw/libcrypto.a']):
dwarfsrcfiles: /home/stackadmin/mallikarjuna/master/build/tmp/work/armv8a-poky-linux/se05x/4.3.1-r0/package/home/root/se05x_mw_v04.03.01/simw-top/ext/openssl/lib_mingw/libcrypto.a: not a valid ELF file
ERROR: Logfile of failure stored in: /home/stackadmin/mallikarjuna/master/build/tmp/work/armv8a-poky-linux/se05x/4.3.1-r0/temp/log.do_package.1040235
ERROR: Task (/home/stackadmin/mallikarjuna/master/sources/meta-test/recipes-se05x/se05x/se05x_4.3.1.bb:do_package) failed with exit code '1'
NOTE: Tasks Summary: Attempted 12233 tasks of which 12232 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
I tried by cleaning both openssl using "bitbake openssl -c cleanall" and compiled se05x recipe, still same error observed.
Please help us to resolve above error and what is reason for the error?
Thanks,
Mallikarjuna Reddy Ambati
Solved! Go to Solution.
Hi @mallikarjuna ,
Please kindly refer to https://community.nxp.com/t5/Secure-Authentication/SE05x-Middleware-04-05-00-do-package-error/m-p/18... for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @mallikarjuna ,
Please kindly refer to https://community.nxp.com/t5/Secure-Authentication/SE05x-Middleware-04-05-00-do-package-error/m-p/18... for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------