New release v04.03.01 on NXP website.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New release v04.03.01 on NXP website.

878 Views
vishwanchandapu
Contributor III

Hi,

A new version of SDK with security updated available on github.
Would like to know if same will be available on NXP website if yes possible ETA.

 

Regards

Vishwa

0 Kudos
Reply
3 Replies

849 Views
vishwanchandapu
Contributor III

Hi @Kan_Li 

Thanks for the response.
One more question as I understand github version is mini package of MW built for Linux.
Is there any specific reason why pkcs11 and access manager is not included?

Regards

Vishwa 

0 Kudos
Reply

843 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vishwanchandapu ,

 

It was just never added. The Openssl engine is also not included in the mini package, and to integrate access manager also JRCP communication layer would need to be supported and switchable in the build configuration which again would add complexity.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 Kudos
Reply

865 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @vishwanchandapu ,

 

Yes, we hope to get the updated Plug&Trust full package this week.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply