Hello @Kan_Li
I have a question regarding the security of the binary files stored on se050 smart card.
I have the following scenario:
1. On the smart card, I created some binary files, each binary file contains some secret information. And I have put a read and write policy on each file using a userID(PIN), so that no unauthorized person can read or write the file.
Now, my question is:
If some unauthorized person gets the access to the smart card, will they be able to read, write or delete the binary files secured with userID (PIN)?
Although I have tried on my end, and I am not able to access those binary files without the knowledge of PIN, but I need a confirmation from some expert from NXP, before I implement these functionalities in my project.
Hope to hear from you soon.
Thank you
Raza
解決済! 解決策の投稿を見る。
Hello @Raza ,
Yes, they will be able to do that if they have the UserID. without knowing this UserID, they won't.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello @Raza ,
Yes, they will be able to do that if they have the UserID. without knowing this UserID, they won't.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------